This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Team,
Our team would love to speak with an applications engineer via online call that could answer some questions we have regarding closed loop control of the DRV8462 and a magnetic encoder using the HW interface of the DRV
Regards,
Visaacan
Hi Visaacan,
Thank you for you interest with the DRV8462 as well as posting your question in this forum. The DRV8462 does not have an HW interface to talk to and work with an magnetic encoder. It is an open loop only stepper driver. However the controlling MCU could interface with the external magnetic encoder for closed loop position control.
In the title you mentioned "dynamically change full scale current depending on load". This can be done with the built-in feature of the device known as auto-torque in SPI control mode without any additional external components. This is described in section 7.3.14 Auto-torque Dynamic Current Adjustment of the datasheet from page-41 as well as in this application note, https://www.ti.com/lit/an/slvaff1/slvaff1.pdf. This feature can be evaluated using one of our DRV8462EVM. Please review these and let us know if any questions. I'm the subject matter expert and application engineer for our stepper drivers portfolio. I can address any questions regarding the DRV8462 via this forum. Thanks.
Regards, Murugavel
Hi Muruagavel,
Yes sorry I was not clear about how everything would be interfaced the plan is to use the HW interface of the DRV8462 (STEP and DIR pins) with an external MCU and the MCU would be communicating with an magnetic encoder to get position data.
One question I had was without using the auto torque feature do you think it is possible to do something similar using the STEP and DIR interface and dynamically adjusting VREF based on encoder data to the MCU, is there other things that we need to consider trying to do an approach like this?
Thanks for the support,
Visaacan
Hi Visaacan,
Thank you for the clarification.
One question I had was without using the auto torque feature do you think it is possible to do something similar using the STEP and DIR interface and dynamically adjusting VREF based on encoder data to the MCU
Yes, you can do this. Changing VREF will change the IFS full-scale current setting. It can be changed dynamically. You want to consider to change VREF at full electrical cycles or half electrical cycles of the current waveform, ideally at the zero crossing. This can be done by keeping track of the number of step pulses which is usually done in the MCU anyways. For example with microstepping current would be a sine wave. Changing VREF at zero crossing would reduce the mechanical artifacts from the motor movement. Thanks.
Regards, Murugavel