Tool/software:
Hello guys,
One of my customers is evaluating DRV8452 for their next products.
[Their conditions]
Micro step:1/32, Toff: Low, Smart Turn Ripple Control mode is selected,
Vref: 1.85V(If=2.8V).
At this moment, they have the following question.
Could you please give me your reply?
Q.
DRV8452 datasheet says that the maximum input frequency of the step signal
of DRV8452 is 100kHz.
Currently, when using the DRV8452 at high speeds, it seems like it cannot keep up with high frequencies.
There is no problem at 16000pps. (16000 x 1/32/200 = 2.5rps = 150rpm)
But at 64000pps, the drive current waveform seems strange. (64000 x 1/32/200 = 10rps = 600rpm)
They think it depends on the motor they use. But they want to know what is the cause of the strange occurred at 64kHz
even though DRV8452 says maximum frequency is 100kHz or higher.
Are the causes the motor inductance and back electromotive force of the motor?
Is there any countermeasure to increase the step clock frequency?
Your reply would be much appreciated.
Best regards,
Kazuya.