This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8329EVM: Motor Speed Control via I2C using STM32-G474RE

Part Number: MCF8329EVM
Other Parts Discussed in Thread: MOTORSTUDIO

Tool/software:

Hi there,

I'm having trouble using I2C with the MCF8329EVM board and an STM32 micro.
the EVM board reacts to I2C commands, but I am unsure of how to set the speed via I2C.


At present, I have been reading the contents of register 0xA4; clearing the lower two bits; and setting them to 0b10, then writing it back to 0xA4.
I then attempt to set the speed via reading the contents of 0xEC; clearing bits 16-30 (var &= ~0x7FFF0000); then placing arbitrary values into the 16-30 bit position.
In addition to setting bit 31 of 0xEC for SPEED_OVER_RIDE then writing back to 0xEC.

I'm not certain what I am doing wrong.

Many thanks in advance,

Best regards,

Nathan