Other Parts Discussed in Thread: DRV8962, DRV8262
Tool/software:
Hello,
I would like to ask if it makes sense to replace ( one DRV8432DKD + mounted heatsink) with ( two in parallel DRV8142DKD heat dissipation over power pad).
The application is a group of 2x voice coils which require a very dynamic control. Each voice coil requires up to 10A. 24V for PVVD.
Any thoughts on this one? I would of course prefer to use only one motor driver, but I don't find any alternative to the DRV8432 in terms of current output.
BR
Afonso