Tool/software:
value | addr |
0x006CAC20 | 0x00000080 |
0xA8200000 | 0x00000082 |
0x048748D0 | 0x00000084 |
0x93112294 | 0x00000086 |
0x143181B8 | 0x00000088 |
0x8BAD1530 | 0x0000008A |
0x216658A2 | 0x0000008C |
0x64590640 | 0x0000008E |
0x0604A6A0 | 0x00000094 |
0x05000000 | 0x00000096 |
0x00000000 | 0x00000098 |
0x800D0000 | 0x0000009A |
0x00000000 | 0x0000009C |
0x00000000 | 0x0000009E |
0xBEE87186 | 0x00000090 |
0xF7C07AB9 | 0x00000092 |
0xA2B3417D | 0x000000A0 |
0x000002A7 | 0x000000A2 |
0x00000009 | 0x000000A4 |
0x00101461 | 0x000000A6 |
0x03E8D00C | 0x000000A8 |
0x3D2E9EC1 | 0x000000AA |
0x9C050079 | 0x000000AC |
0x00000556 |
0x000000AE |
Hello, I now have a question, the product configuration is as above, I need to achieve the accuracy of 2% of the current limit, how to meet the requirements, at this stage can only reach 5%, it is more difficult to get.