Tool/software:
I have a follow up question for the E2E thread listed below:
https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/1071091/drv8876evm-run-tec-with-lc-filter
I am trying to filter PWM using an LC filter as described in the above E2E thread.
I have two questions:
1) Can I disable the Over-Current protection of the DRV8876? The data sheet states:
The internal current regulation can be disabled by tying IPROPI to GND and setting the VREF pin voltage greater than GND (if current feedback is not required).
however, it isn't clear to me if this disables the over-current protection and fault?
In other words, if I tie IPROPI to GND and VREF > GND would I be able to use output capacitors that are 100uF without faulting?
2) It states that the maximum PWM frequency is 100kHz. Is this limit due to OCP requiring a minimum on time of 3us, or for some other reason?
what would happen if I ran this part with a 250kHz switching rate?
Thanks