This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8262: Oscillations occured when driving a TEC

Part Number: DRV8262

Tool/software:

When a TEC is driven in the DRV8262 PWM mode, the output voltage of the LC filter behind the OUT terminal exceeds the voltage value of the VM.  It looks like an oscillation, but what is the cause of it?

  • Hi Liu,

    Thank you for posting in this forum. It may be likely the L-C in your schematic and the PWM frequency may be resonating. Please share the schematic, VM voltage information, PWM control sequence, fPWM used and the TEC load characteristics. The DRV8262 does not oscillate, other than outputting the input PWM frequency. See this e2e post.

    Regards, Murugavel 

  • Hi Murugavel,

    Thanks for your reply. 

    The schematic is below. The VM voltage is set to  20V,  the frequency of PWM is 100KHz and the TEC is about 2ohms. The inductance in the LC filter is 47uH, the capacitance is 22uF.

    Best, 

    Liu

  •  one in IN1 and IN2 has a continuous input high and the other input PWM.

  • Hi Liu,

    Thanks for the additional info. The LC filter has a low pass transition at 5 kHz which is good and filters the 100 kHz PWM effectively. Was J9 pins1-2 shorted during the waveform capture? If not try capturing the waveforms with 1-2 shorted, no current regulation. The duty cycle of the PWM will set the TEC current.    

    See below scope capture done with an DRV8262EVM connected to a TEC load. with similar LC filter in the schematic you shared. The yellow trace is on  OUTx side of the DRV8262, the green trace is the voltage waveform after the inductor and on one of the capacitors, the blue trace is the TEC current, 100 kHz PWM 50 % duty cycle. Current regulation was disabled. There was no abnormalities observed with the waveforms.  

    Based on the schematic you shared, the device is configured as Single H-Bridge in PWM control mode. In this mode below control sequence must be followed. While the TEC is not driven both IN1 and IN2 must be logic high. For driving with PWM input depending on the polarity one of the inputs must be high and the other input must be PWM input. The TEC load would be active during PWM off time. This is the control logic. Please verify and make sure you are following this control logic. Please also capture VM voltage and check if there are any abnormalities with it. 

    one in IN1 and IN2 has a continuous input high and the other input PWM.

    I assume this was what you meant by this. We do not see any abnormal output while replicating your setup with a DRV8262EVM. Thank you.

    Regards, Murugavel 

  • Hi Murugavel,

    Thanks for your reply. The output returns to normal when J9 is shorted. 

    Best,

    Liu

  • Hi Liu,

    Thanks for the update. I'm glad the issue was resolved. 

    Regards, Murugavel