I have been testing the DRV8825 with a 2A stepper motor running at full power on 24V.
I have been trying to get smooth low speed rotation, by using 32 step mode.
I seem to be getting some 'cogging' where the motor progresses smoothly through the 32 steps until the end when it suddenly jumps.
This makes movement a bit jerky.
Is this a function of the drive or the motor? I am guessing that the motor is jumping to the next full step position?
The effect is less obvious at 1/16th step and dissapears at 1/8th, but at these settings there is too much vibration in the drive so I really want to use 1/32 mode.