Hi I am currently trying to use the DRV8843 to drive two DC motors that can consume up to about .5 A when fully loaded. I am essentially using the same logic as the diagram on page 2 of the datasheet, and I have nReset and nSleep tied to +5V, and Decay left floating. I'm not using the current sense pins and have tied those to ground. After an hour or so of testing my application, the chip no longer seemed to work. I checked a few of the pins and the 3.3V regulator output was no longer giving 3.3, and instead just stuck at ground. I was having it directly drive the VREF pins, however after soldering a new chip on I disconnected it completely, instead using a simple voltage divider for the VREF pins. Any suggestions as to why this would happen?