This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HC Motor control kit

Other Parts Discussed in Thread: DRV8301

Hi everybody on TI forum,

                                             This is Siva, am actually working with a 24 Volts 8A BLDC motor in the High current motor control kit with F28069 and DRV8301 combination. It works well when trying it with Motor ware GUI. But i got strucked when i planned to proceed it with a example code which is given for F28069 controller in the control suite. I configured the program for BUILD LEVEL 7 and changed the motor parameters in the program and worked following the instaspin incremental build manual. It is asked to enable the flag and change the ISW values in the watch expression. when i change the ISW value to 1, the motor starts jerking but not running. what might be the problem? and how to fix this problem? It will be so good if i get a solution very soon.

Regards,

Siva.V.Girish