Hi, I am a newbie to this forum and would like to ask 2 questions.
1) I would like to do regenerative braking on the DRV8312-69M-KIT (haven't purchased yet). Is this possible in terms of hardware? I have looked at the schematics and the power input is a 24V constant DC supply. In future, I would replace this DC supply with a battery, so I would like to know whether the power flow can be reversed during regenerative braking in terms of hardware.
In terms of software, I have read this thread and some customization is required in the MotorWare software in order to do regenerative braking, am I right?
http://e2e.ti.com/support/microcontrollers/c2000/f/902/t/273438.aspx
2) My 2nd question is: how do I scale down a speed-torque-time curve for use on a small motor?
I have a speed-torque-time curve for a full-size electric vehicle (EV). This has been derived from a speed-time drive cycle. By considering the mass of the car, slope gradients, and acceleration required, etc, the torque-time curve can be calculated.
The full-size EV motor is supposed to follow this speed-torque-time drive cycle so we can evaluate its performance. Now, I would like to scale down this speed-torque-time graph so it can work on the DRV8312-69M-KIT for small scale experiments. I have done some googling and I can't seem to find how I can scale it down. Can it be scaled down linearly?
In future, I may also buy another motor to function as the load torque. Thanks in advance for any help!