This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi B.R,
DRV11873 is intended for applications where motor is running all the time. You can certainly use DRV11873 to move to desired position but you will need other ways to hold the desired position.
Thanks,
Seil
Hi Seil,
Thanks for your response, I use gimbal motors as a direct wheel motors in my robot. questions:
Sorry, I know they are too many questions ;)
B.R.
Salvador
Hi Salvador,
Please see comments below:
Can I disconnect power to the motor with DRV11873? Is there an enable signal?
[KS] You can use PWMIn pin, when this pin is driven to 0 V(GND) it will stop driver.
Can I use a one of the three fases to stop the motor?
[KS] Can you please elaborate question here
I need slow motion from zero rpm to start the motion of the robot, and I need too: free wheels for free movement and zero energy comsuption and in the other hand stop the wheels powering the magnets of the motor without squence, is there another better option as blcd driver?
[KS] Another 12 V integrated BLDC driver I would recommend is DRV10975, DRV10975 has EEPROM which can be configured to have different startups profile and so on.
Regards,
Krushal