This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have successfully gotten the DRV11873 running with a hard drive motor. My PWM is 28 KHz and I run it at 12 V. The current resistor is 1 K and in lowspeed.
The problem is when the device is powered up I put a ramp on the PWM. But the DRV spinns up the motor to a high speed and then regulates down to the PWM supposed speed. My duty cycle is just about 6 %.
How can correct this or this or is this device related behavior? I already tried other voltages but there is no difference.
Thanks!
Best regards