This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8803: Operating Temperature issue

Part Number: DRV8803
Other Parts Discussed in Thread: DRV8860, DRV8802

Dear Sir,

We are using DRV8803 for relay driving.

When we refereed the datasheet we found that operating temperature  mentioned was –40  to 85 °C and also in Absolute maximum rating it is mentioned as Operating virtual junction temperature(Tj) –40  to 150 °C.

So which temperature we should consider kindly help us. Because we are in need of extended temperature  105 °C or 125 °C

Regards

Girish

em electronix