This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
We are using DRV8803 for relay driving.
When we refereed the datasheet we found that operating temperature mentioned was –40 to 85 °C and also in Absolute maximum rating it is mentioned as Operating virtual junction temperature(Tj) –40 to 150 °C.
So which temperature we should consider kindly help us. Because we are in need of extended temperature 105 °C or 125 °C
Regards
Girish
em electronix
Dear Rick Duncan,
Thanks for your reply,
Current required by relay is only 85mA so there is no problem for usage of DRV8803. Our only concern is the operating temperature since we want use it as extended temperature of 105 Deg, C.
Girish
Dear Rick,
You have said power is less than 2% of the rated power and device will work with little increase in junction temperature . Kindly specify the what is little increase temperature pl. specify the temperature
Girish
Dear Rick Duncan,
Thanks for your reply.
Kindly tell me if all channels are ON with each channel sourcing 85mA-100mA current, what will be the overall wafer temperature(IC operating temperature) with ambient temp.
Regards
Girish
Hi Girish,
Power through the outputs at 100mA is I2R x 4, or .032W. Additional power is used to run the device and can be estimated as VM * 2.1mA.
Assuming VM = 24V, it should be <40C, but this depends on board design and package used.
Quick calculations can be done by going to www.ti.com/.../midlevel.tsp
Select the DRV8802. The DRV8802PWP package has similar thermals as the DRV8803PWP thermals.
A rough estimation for the DRV8803DW package is roughly double the PWP.