This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8841: Why DRV8871 is not suitable for solenoid driving

Part Number: DRV8841
Other Parts Discussed in Thread: DRV8871,

Dear Sir/Madam,

When looking at TI motor control brochures, I noticed that it mentioned DRV8841/8842 is suitable for solenoid driving but DRV8871 is not. Why is the reason?

my end application is for safety device, and PCB size is small. So reluctance to use DRV8841/8842  although they are good however the size is quite big. What would be the pros and cons if I use DRV8871/72 for driving solenoid?

  

Best Regards,

kpk