I have a new board design and I'm trying to debug why the DRV8880 immediately issues a fault. If I toggle the enable pin and trigger on the fault pin I can see it being 3.3V for less than 3us. I've measured all the pin voltages and I don't see any reason for the part to go into fault but every time I power up or toggle the enable pin it immediately goes into fault. Perhaps I have something wrong in my design that I'm not seeing? I've attached the schematic and the spec on the motor being used.
Here's what I measure on each pin
Name | Pin # | Voltage (V) |
CPL | 1 | 0.133 |
CPH | 2 | 23.4 |
VCP | 3 | 35.7 |
VM | 4 | 23.9 |
AOUT1 | 5 | 0 |
AOUT2 | 7 | 0 |
AISEN | 6 | 0 |
BOUT2 | 8 | 0 |
BOUT1 | 10 | 0 |
BISEN | 9 | 0 |
ATE | 13 | 3.3 |
VREF | 14 | 1.05 |
V3P3 | 15 | 3.3 |
TOFF | 16 | 0 |
nSLEEP | 17 | 3.3 |
nFAULT | 18 | 0 |
DECAY1 | 19 | 0 |
DECAY2 | 20 | 0 |
ENABLE | 21 | 3.3 |
DIR | 22 | 0 |
STEP | 23 | 0 |
M1 | 24 | 0 |
M0 | 25 | 0 |
TRQ1 | 26 | 0 |
TRQ0 | 27 | 0 |
Thanks in Advance,
George