Tool/software: Code Composer Studio
Hello,
I'm working with the DRV8312EVM developped kit with the motor BLDC DT4260-24-005 24VDC 4000RPM (just starting). I ran the example code BLDC_sensorles, the motor runs just untill the level 4. AT level 5, when I close the loop, it didn't work. I think the problem coule be in the CMTN_TRIG module.
Below is the CmtnTrig and ZcTrig signal mesured. I think is not normal comparing with the guide file (which say that CmynTrig should appear 30° after the ZcTrig). the motor in this case still works.
Thank you in avance for your support,
Trung