Part Number: DRV8432
Hi,
I'm using DRV8432-EVAL module in PFB(parallel Full Bridge) Mode to drive Peltier module rating 24V/12A.
I have worked on My own designed DRV8432 PCB in PFB mode. myschematic design also attached here.
The board is working good PVDD=12V driving 4A current.Peltier-Driver-DRV8432-schematic.pdf
if voltage is changed to PVDD=15V trying to drive 6A current and IC 8432 and heat sink are getting too hot and finally driving 1.8A of current showing 5V(30% DC) on output though the PWM is 98% (DC).
Mode: PFB
PWM Freq : 40Khz
1 . Peltier - heating
PWMA - 98% Duty Cycle
PWMB -1% DC
2. Peltier - cooling
PWMA -1% DC
PWMB - 98% Duty Cycle
Why cause this? How to solve this problem?
Thanks
Regards
Sai