This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2605L: 5 or more LRAs into the 1 DRV2605L

Part Number: DRV2605L
Hello. I am thinking to add vibration feedback to a touchscreen display, but the issue is that display was not specially designed for haptic motors. (i.e. I can see in TI example project LCD/touchpanel is floated so that vibration is effectively spread on its surface, but with ordinal monitors LCD panel is firmly attached to the sloid and relatively heavy background.) I learned that adding more haptic motors (instead of just one, maybe 5 or more) may help to vibrate the whole chassis and I want to try this. Then my question is is there recommended circuit connection and/or number of drivers. e.g.: - One DRV2605L chip connected to multiple motors? - Multiple DRV2605L chips each connected to a motor? I imagine motor power consumption or like may force some design restriction but I am new to electri circuit designs.