This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I saw that DRV8832 has an efficiency parameters but the DRV8837 does not have it.
How can I get these parameters? From a short test I ran I get low efficiency at 5V operation with a 27Khz PWM and 100mA DC Brush motor consumption.
Part Number: DRV8837
Hi,
I ran the same scenario for both TI drivers with 3xAA batteries connected to TI DC booster TPS63050
In both cases I ran the eval boards with the same VM of 5V.
On both I choose a 50% duty cycle so motor will run in 2.5V.
Running both till total battery depletion.
DRV8832 ran for 23.5 hours
DRV8837 ran for 17 hours
Am I missing anything here? After all DRV8832 has a higher RDSon + Rsens.
One more issue is about the internal shoot through protection, does it have it?
Thanks,
Tzion
Tzion,
For battery-powered applications, the main device specs that I could see affecting efficiency are operating current and Rds(on).
The total operating currents of the two devices are similar, according to the datasheets (1.4 mA for DRV8832, and 0.7+0.8 = 1.5 mA for the DRV8837). However, the DRV8832 may draw additional current if you have a resistor on the VREF pin. Overall, I would not expect this difference to cause a 6-hour reduction in battery life.
In terms of power dissipation, the Rds(on) and sense resistors will be the biggest points to dissipate power before it even gets to the load. The DRV8832 has almost twice the Rds(on) (LS+HS = 450 mOhm) compared to the DRV8837 (LS+HS = 280 mOhm). Considering this data, I would expect the efficiency of the DRV8832 to be worse if we calculate efficiency as electrical power out divided by electrical power in. However, the power dissipated by the FETs in either device is < 5 mW compared to the 250 mW power dissipation by the motor. Also, the difference in the power dissipation between the two devices should not cause a 6-hour difference in operating time over a 24-hour testing period.
I think that the reason you are seeing this discrepancy in your battery lifetimes is because AA batteries can vary in their capacity. You may also want review your prototype boards for other possible current leakage paths that may contribute to this discrepancy.
Edit: Fixed typos
Hi James,
I think there is a small confusion.
DRV8832 has a P-Channel and N-Channel and has HS+LS=450mΩ + Sense resistor (0.2Ω)
DRV8837 has dual N-Channel and so it has HS+LS=280mΩ
So DRV8837 should be better and more efficient although the test results show different?!
Tzion
Hi James,
So from what I read between the lines you don't expect almost any differences between these 2 motor drivers?
I ask a lot on this because the DRV8837 is much cheaper and my project is very tight on cost but w/o compromising on quality (healthcare product).
We saw that the DRV8837EVM consumes about 5mA with no load (MCU + LED), so we removed the 5mA from the results of the DRV8837 and the results become much closer to each other.
I will send you the Excel file and graphs.
Tzion