This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10987: Please Help ! DRV10987 DELAY START problem

Part Number: DRV10987

Hello Ti team,

I am using DRV10987 for my smart car application.And now I can spun my motor successfully.But i find a serious problem is that DRV10987 can't work after writing EEPROM(Writing SPEED command  into EEPROM after Motor configration). And few second ago motor with spun up...(Power on and Motor didn't spun)

I measured Kt value of motor is about to 10mv/hz(average)  , Rph is 3.5R , No IPD , ISD enabled , No break .I set registers as following code , could you please help me find where the problem is?

void DRV_init(void)
{

		i2c_init(i2c0,100*1000);

		i2c_init(i2c1,100*1000);
 
		systick_delay_ms(1);				//Wait for set up 1ms


		do
		{

			i2c_write_reg(i2c0,DRV10987_Address,EECRTL,0x80,0x00);				//Setting EEPROM Access permission and DISABLE!!!!!!!! the motor

			i2c_write_reg(i2c0,DRV10987_Address,EEPROM1,0x00,0x00);				//clearer EEPROM Access code

			i2c_write_reg(i2c0,DRV10987_Address,EEPROM1,0xC0,0xDE);				//Setting EEPROM Access code

			gpio_init(G0,GPO,0);
// 
//			systick_delay_ms(1);				//Wait for set up 1ms

		}while(i2c_read_reg(i2c0,DRV10987_Address,EEPROM2) != 0x0001);		//Setting EEPROM able to read

			gpio_init(G0,GPO,1);

		i2c_write_reg(i2c0,DRV10987_Address,CONFIG1,0
																								| NO_SpectrumControl_MASK
																								| FG_both_open_and_close
																								| FG_Only_Close
																								| FG_POLES(16),
																								0
																								| CLK_ADJ_SELECT(0)		  //0:FULL 1:HALF
																								| 0x5B );								//Setting to 3.5R


		i2c_write_reg(i2c0,DRV10987_Address,CONFIG2,0
																								| 0x0F,									//Page 24
																								0
																								| CommAdvMode(1)					
																								| 0x02 );									//Page 37
		
		
		i2c_write_reg(i2c0,DRV10987_Address,CONFIG3,0
																								| ISDThr_160ms
																								| BrkCurThrSel(0)
																								| BEMF_HYS(0) 
																								| ISDEn(1) 
																								| RvsDrEn(0)
																								|	RvsDrThr_6P3,								
																								0
																								|	OplCurr_0p4			
																								| OplCurrRt_6
																								| BrkDoneThr_0 );							

		
		i2c_write_reg(i2c0,DRV10987_Address,CONFIG4,0
																								| AccRangeSec(0)
																								| StAccel2(0)
																								| StAccel(0),								
																								0
																								|	Op2ClsThr(1,6)			
																								| AlignTime(6) );

		i2c_write_reg(i2c0,DRV10987_Address,CONFIG5,0
																								| OTWarmingLimit(0)
																								| CloseLoopStuckLock(0)
																								| OpenLoopStuckLook(0)
																								| NoMotorLock(0)
																								| AbnormalKtLock(0)
																								| AbnormalSpeedLook(0),								
																								0
																								|	SWiLimitThr(0)			
																								| HWiLinitThr(0) 
																								| IPDasHWlLimit(0)  );


		i2c_write_reg(i2c0,DRV10987_Address,CONFIG6,0
																								| SpdCtrlMd(1)
																								| PWMFreq(1)
																								| KtLckThr(0)
																								| AVSIndEn(0)
																								| AVSMMd(0)
																								| IPDRIsMd(0),								
																								0
																								|	CLoopDis(0)			
																								| CIsLpAccel(3) 
																								| DutyCycleLimit(3)  
																								| SlewRate(3)  );


		i2c_write_reg(i2c0,DRV10987_Address,CONFIG7,0
																								| IPDAdvcAg(0)
																								| IPDCurrThr(5)
																								| IPDClk(4),								
																								0
																								| CtrlCoef(4)  
																								| Deadtime(10)  );

		
		i2c_write_reg(i2c0,DRV10987_Address,EEPROM5,0x00,0x06);

		while(i2c_read_reg(i2c0,DRV10987_Address,EEPROM2) != 0x0001);

		i2c_write_reg(i2c0,DRV10987_Address,EEPROM5,0x00,0x02);

		while(i2c_read_reg(i2c0,DRV10987_Address,EEPROM2) != 0x0001);

		i2c_write_reg(i2c0,DRV10987_Address,EECRTL,0x00,0x00);

/***********************************************************************************************************************************************/

		do
		{

			i2c_write_reg(i2c1,DRV10987_Address,EECRTL,0x80,0x00);				//Setting EEPROM Access permission and DISABLE!!!!!!!! the motor

			i2c_write_reg(i2c1,DRV10987_Address,EEPROM1,0x00,0x00);				//clearer EEPROM Access code

			i2c_write_reg(i2c1,DRV10987_Address,EEPROM1,0xC0,0xDE);				//Setting EEPROM Access code

			gpio_init(G0,GPO,0);
// 
//			systick_delay_ms(1);				//Wait for set up 1ms

		}while(i2c_read_reg(i2c1,DRV10987_Address,EEPROM2) != 0x0001);		//Setting EEPROM able to read

			gpio_init(G0,GPO,1);

		i2c_write_reg(i2c1,DRV10987_Address,CONFIG1,0
																								| NO_SpectrumControl_MASK
																								| FG_both_open_and_close
																								| FG_Only_Close
																								| FG_POLES(2),
																								0
																								| CLK_ADJ_SELECT(0)		  //0:FULL 1:HALF
																								| 0x5B );								//Setting to 3.5R


		i2c_write_reg(i2c1,DRV10987_Address,CONFIG2,0
																								| 0x0F,									//Page 24
																								0
																								| CommAdvMode(1)					
																								| 0x02 );									//Page 37
		
		
		i2c_write_reg(i2c1,DRV10987_Address,CONFIG3,0
																								| ISDThr_320ms
																								| BrkCurThrSel(0)
																								| BEMF_HYS(0) 
																								| ISDEn(1) 
																								| RvsDrEn(1)
																								|	RvsDrThr_6P3,								
																								0
																								|	OplCurr_0p8			
																								| OplCurrRt_6
																								| BrkDoneThr_0 );							

		
		i2c_write_reg(i2c1,DRV10987_Address,CONFIG4,0
																								| AccRangeSec(0)
																								| StAccel2(0)
																								| StAccel(0),								
																								0
																								|	Op2ClsThr(1,6)			
																								| AlignTime(6) );

		i2c_write_reg(i2c1,DRV10987_Address,CONFIG5,0
																								| OTWarmingLimit(0)
																								| CloseLoopStuckLock(0)
																								| OpenLoopStuckLook(0)
																								| NoMotorLock(0)
																								| AbnormalKtLock(0)
																								| AbnormalSpeedLook(0),								
																								0
																								|	SWiLimitThr(0)			
																								| HWiLinitThr(0) 
																								| IPDasHWlLimit(0)  );


		i2c_write_reg(i2c1,DRV10987_Address,CONFIG6,0
																								| SpdCtrlMd(1)
																								| PWMFreq(1)
																								| KtLckThr(0)
																								| AVSIndEn(0)
																								| AVSMMd(0)
																								| IPDRIsMd(0),								
																								0
																								|	CLoopDis(0)			
																								| CIsLpAccel(3) 
																								| DutyCycleLimit(3)  
																								| SlewRate(3)  );


		i2c_write_reg(i2c1,DRV10987_Address,CONFIG7,0
																								| IPDAdvcAg(0)
																								| IPDCurrThr(5)
																								| IPDClk(4),								
																								0
																								| CtrlCoef(4)  
																								| Deadtime(10)  );

		
		i2c_write_reg(i2c1,DRV10987_Address,EEPROM5,0x00,0x06);

		while(i2c_read_reg(i2c1,DRV10987_Address,EEPROM2) != 0x0001);

		i2c_write_reg(i2c1,DRV10987_Address,EEPROM5,0x00,0x02);

		while(i2c_read_reg(i2c1,DRV10987_Address,EEPROM2) != 0x0001);

		i2c_write_reg(i2c1,DRV10987_Address,EECRTL,0x00,0x00);

		systick_delay_ms(50);				//Wait for set up

			
} 

void DRV_set_speed(uint8 DRR, uint16 speed)
{
		 uint8 MSB,LSB;

		 MSB = (uint8) ( ( (speed >> 8) & 0x0001 ) | 0x80);

		 LSB = (uint8) ( speed & 0x00ff );

			
		 if(DRR==0)      i2c_write_reg(i2c0,DRV10987_Address,SpeedCrtl,MSB,LSB);
		 else if(DRR==1) i2c_write_reg(i2c1,DRV10987_Address,SpeedCrtl,MSB,LSB);
		
}