Other Parts Discussed in Thread: CSD18540Q5B, DRV8702-Q1EVM
The kit worked great once I found that the Sleep Button state was backward. I assumed Enabled was to drive the signal low. After using a DMM I found that the state was backwards. Once this was resolved the kit worked well.
Observations:
I am using a 24 volt motor with a 24 volt power supply. The test configuration was using the motor to lift 50 pounds of weight. I used a clamp current meter to measure the current during the test process. The current meter read 1 amp greater than the EVM software. I saw a high current of 4.9 Amps during the raising of the weight and the holding current to maintain the weight was 3.0 Amps. During the holding time I felt the FETs and was surprised by the heat dissipation. I am concerned that the FET will not be able to hold the weight for an extended period of time (months, years). I reviewed the FET's datasheet and found that they are very robust and should be able to handle my application. Below is the part number of the FET used on the evaluation board.
| MOSFET, N-CH, 60 V, 28 A, SON 5x6mm |
| CSD18540Q5B | Texas Instruments |
Question #1:
Has anyone else seen the reverse behavior of the Sleep Button?
Question #2
Was the evaluation board designed with significant heat dissipation to drive high current for 5 Amps?
Thank you
Rob Cohen
Smoke Guard