Dear, Sir.
My customer is evaluating DRV8703-Q1. During that, They are facing following
symptom on /SLEEP & /FAULT.
/FAULT Glitch(LOW) during aprox. several 100us ~ 1ms can be observed at
/SLEEP LOW<=>HIGH.
1. Is it a normal behavior which DRV8703-Q1 has?
2. If it was normal, Is it possible to define maximum duration of /FAULT=LOW?
Considering the solution such as doublle reading by MCU, the duration would
be significant. Please give your advice.
Best Regards,
H. Sakai