This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8703-Q1: LOW-->HIGH nSLEEP pin transition

Part Number: DRV8703-Q1

Hi everyone, I have a doubt about t(WAKE) time.
From datasheet I read "The DRV870x-Q1 device is brought out of sleep mode automatically if the
nSLEEP pin is brought high.The t(WAKE) time(1ms) must elapse before the outputs change state after wakeup."
I would like to know if after that nSLEEP is set HIGH, it is possible to use immediately SPI or it is necessary to wait 1ms.
1ms is referred also to output state change or to the time to wake up the device?
Thanks a lot.
Anita