Part Number: DRV110
Hello team,
Can Ipeak and Ihold set to 1A, 330mA?
In the datasheet, current is set by Vref and Rsense and Vref is set by resistor.
Recommended resistor value is from 66.67k~2M and 66.67k~333k and if Rsense is 1Ohm, maximum peak is 900mA.
If Rsense is below 1Ohm(for example 0.5Ohm), can Ipeak and Ihold set to 1A and 330mA?
Thanks.