I tried DRV8812 with DECAY pin driven high, and this clarified that decay mode in DRV8812 can be selected to be slow/fast ONLY DURING CURRENT CHOPPING; outside this case, decay is FIXED FAST , as it can be seen from scope traces in attachment.
One of the consequences of this device behaviour is that DRV8812 CANNOT BE USED TO DRIVE DC MOTORS in PWM mode, typically used to drive a DC motor (mode that is quite different from PWM mode for stepper motor),
This is not clear at all from data-sheet and moreover "capable of driving 2 DC motors" in features list is very misleading...
Is there any work-around to avoid fast decay when PWM = xENBL pin goes low? I need a very urgent answer
Thank you for your anser. BR
Maurizio