DRV8323 cannot drive normal Level FETs in case the DC link has gone down to e.g. 7V
What would happen in case we would build in a step-up Converter to Supply the IC with minimum 13V?
In that case we would have enough Voltage to allow operation of the normal Level FETs.
But then we have the problem that the PIN VM of the IC is higher than the PIN VDRAIN.
è Will it cause some issue e.g diodes conducting in the Chip
è Will VDC monitoring work?
Best wishes,
Olrik