This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8803: connecting tho inputs and two outputs parallel

Part Number: DRV8803

Hi,

Would it be possible to connect two inputs like IN1 and IN3 in parallel and to the same with the outputs Out1 and Out3 to increase the current capacity?

I was thinking of connecting IN1-IN3 and Out1-Out3  
and also connecting IN2-IN4 and Out2-Out4

For an application I would need 1[A], so I was hoping to solve this by connecting it in parallel.