Other Parts Discussed in Thread: DRV10975, DRV10987, DRV10974, DRV11873
I am having the same problem as previously brought up. I have a 12 V BLDC motor, but when I hook it up to the driver it pulses a few times with decreasing torque and then stops for a few seconds before repeating. I tried 2 boards on 2 different motors with 2 power supplies one a 12V, the other variable voltage between 5 and 12V. I also tried removing the J2 jumper, this made the pulses happen at higher frequency, but no other change.