This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Wang,
When I connected the valves to the outputs of the DRV8844EVM and turned on the valves, I noticed that there are around 350mA current drawing from the power supply. I thought the the DRV8844 would take ~3mA as input supply current, and will provide the output current the valves via CP and reg in the driver. Is that correct?
Thanks,
Nhi
Nhi,
On the EVM, there is several other ICs on the board. To find out the DRV8844 current, you can compare the current with nSLEEP pin low and nSLEEP pin high.
The 3mA current supports charge pump, reference and other internal circuit. The valves current goes through VM to OUTx.