Other Parts Discussed in Thread: CSD18531Q5A
When trying to drive a two-phase stepping motor with DRV8711, a phenomenon occurred in which the position accuracy of the motor fluctuated from step to step.
As a result of the investigation, the current flowing through the motor is different between the A phase and the B phase, and the stop position seems to differ depending on the excitation state.
The set drive current is 0.7A. However, there is a difference of about 50mA at 718mA for phase A and 665mA for phase B.
The driving conditions are as follows.
・VM : +48V
・Excitation Mode : 2-Phase(Full step)
・Drive Current : 700mA (TORQUE = 15, ISGAIN = 5, RISENCE = 33mohm)
・Decay Mode : Mixed Decay(all time)
・External FET : CSD18531Q5A(TI)
1. Is there a possibility that this difference in current will occur in device performance?
2. Is there a way to correct the current value for each phase?
Best regard.