Part Number: DRV2700
Dear Specialists,
we would be grateful if you could advise。 How to use DRV2700 for piezo driver with High voltage(1000V ac@flyback mode) and we have some questions and want some design information(For example: calculation of parameter design,but the user guide is not given ).
According to the datasheet P.12 8.4.2 Flyback Mode, DRV2700 can drive 1000V output by using Flyback mode,but "slou407a" user guide is not given about transformer design information,only feedback network parameter modification is given.then we use the TINA-TI Reference Design "slom404.tsc",we aslo couldn't find 1000V output(about 600V) by feedback network parameter modification(R5 is changed from 5.11k to2.56k, C5 is changed from 8.2nF to 16.2nF,the other parameters remain the same).
we questions as foollow :
1. I'd like to know about transformer, because I couldn't find 1000V output by Flyback mode.
2. how to choose transformer saturation current ,turns ratio and inductance value , etc ? Reference Design "slom404.tsc" is simple inductance and mutual inductance,we want to know transformer parameter for 1000V output by Flyback mode.
3. Is also there a detailed user's manual for the design of 1000v output by Flyback mode, which contains the calculation of the whole Flyback mode circuit parameter design, we want do WCA (Worst case analysis) .
I appreciate your great help in advance.
Best regards,
yunbai qin