Other Parts Discussed in Thread: DRV2604, DRV2624
1、The preset effects contain three parts: Overdrive, Sustain, brake. Can I set these four parameters (ODT,SPT,SNT,BRT) to extend the duration of the vibration without changing the Overdrive and brake? (for example, the default duration of strong Click effect is 65ms. Can I extend it to 1000ms? This can be done in RTP mode, but there are no Overdrive and brake parts.
2、If I can adjust the duration of embedded haptic effects. Which parameter do I need to adjust to extend the duration of vibration and how to set?
Thank you very much for your excellent engineers. My technical level is limited, but I am in a hurry to achieve the goal. I hope to get your help. Thanks again!