Other Parts Discussed in Thread: DRV8323
Hello,
we developed for our customer DC motor CAN controller based on DRV8703. This controller is designed for 12V or 24V supply voltage. Now, our customer's reuest is nominal voltage 48V (13S32P Li-Ion accu - 55V fully charged) and limitation of DRV8703 is 45V. Do you have some recomendations in propper driver selection? I found DRV8323RS which is intended for BLDC. This part contain three half bridge gate drivers. Can I use only two of them? If yes, how to connect unused pins (GHC,SHC,GLC,SPC and SNC) with respect to propper functionality of internal protection and fault indication bits?
Thank you for your kind answer in advance.
Best Regards,
Ladislav