Other Parts Discussed in Thread: CSD18531Q5A
Hi Rick,
do you have any answers for my past questions?
Here's the IDRIVE and TDRIVE settings in the original design:
The FET used has QG(tot) total gate charge 12.5 nC @ ID = 15 A; VDS = 40 V; VGS = 10 V.
We wanted the RT rise time shorter than 300ns (for low power losses and shorter than the minimum dead time of 400ns)
IDRIVE > Q / RT; 12.5nC/300ns=42mA (50mA is the minimum pre-drive current of the driver)
TDRIVE > 2 × RT; 2x300ns=600ns
As the rise time was measured less than 200ns, TDRIVE = 250ns was set. Today I see that a longer TDRIVE would be better for fully charge the gate.
Is it possible that switching off the pre-driver before reaching full gate voltage could cause a gradual degradation of the DRV8711 gate holding current source?
On the A2HS driver of the DRV8711 test piece, I noticed a reduced gate driver voltage to 8V, while the other drivers of the test piece give 9.5V. Could this be a sign of the beginning degradation of DRV?
Thank you in advance for your answers.
Michal