Part Number: DRV8812
Other Parts Discussed in Thread: DRV8832, DRV8412
Fur a new project for one of our customers we need to control a climate chamber by a Peltier module. Probably we will need a module with at least 100W cooling capacity (+24V module).
I found the DRV8812 or DRV8832 that should be suitable to control such modules and I found an application sheet for a TEC driver in your datasheet. However some questions about this :
1) Is it possible to reverse the voltage at the TEC with this module because we need to cool down and heat up. Or do we need additional electronics when we want to reverse the Peltier current?
2) I found different applications and comparisons between PWM and linear control (direct current) where the PWM control is very inefficient compared with linear control. So I was wondering if t.I has examples of linear control of a TEC. Or do you think the efficiency with a DRV8812 (or DRV8832) is quite well?
3) Do you know if there are standard controller chips for controlling the DRV8812 or is it possible to control this directly from an embedded PC (e.g. with I2C or SPI PWM controller)
Regards
Chris van der Aar
NTS Systems Development
Eindhoven, The Netherlands