This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8306: duty cycle resolution

Part Number: DRV8306

Hi, What is the duty cycle resolution for the PWM control input to the DRV8306? So for example if I have a PWM at 20kHz and I adjust the duty cycle from 50% to 50.01%, will the commanded speed change? Thanks.