This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8353RS-EVM: What happens if I connect and run 60 degree HALL sensor placed motor ?

Part Number: DRV8353RS-EVM
Other Parts Discussed in Thread: DRV8353

Hi,

Please let me know, will DRV8353 chip fails if I connect and run 60 degree placed (instead of 120 deg) HALL sensor motor 

From datasheet I could see DRV8353 supports 120 deg HALL placement,

is there any safety mechanism in DRV8353 which prevents damage of chip if I connect and run 60deg HALL motor ?

thanks,

Chandra

  • Chandra,

    How many sensors does this motor have? Can you share the motor datasheet?

    Regards,

    -Adam

  • Hi Adam,

    Sorry for late reply,  I couldn't get its datasheet

    This motor has 3 HALL sensors, each placed 60 deg apart.

    Question is, will DRV8353 handle both 60 deg and 120 deg placed HALL sensor motors safely ?

    thanks, Chandra..

  • Chandra,

    The DRV8353 can only work with 120 degree hall sensors, you would need to use the MCU with the 60 degree hall sensors and then use the MCU to drive the hall sensor inputs with the phase adjusted for 120 degree operation. 

    As a reminder, 3 of 60 degree hall sensors only cover 180 degrees of the circle, or half of 360 which is what 3 sensors at 120 each will cover.

    Regards,

    -Adam

  • Hi Adam,

    Thank you for the information

    I found a workaround below for correcting the phase of 60 deg HALL sensors to 120 deg, please let me know is below a perfect solution

    120deg Hall Effect Sensors:
    The following diagram shows 120-degree hall-effect sensors. Notice that there is electrically 120 degrees between hall transitions.

    60deg Hall Effect Sensors:
    The following diagram shows 60-degree hall-effect sensors. Notice the Hall 3 signal is inverted (compared to 120-degree hall3) This changes the number of electrical degrees between the rising edge of the hall states.

    All of the hall motors Compumotor uses are 120degrees. If we use an inverter on Hall 3 we can change a 60degrees hall state to 120degrees and vise versa.

    Request you confirm with your ASIC team that above workaround is good enough to make it work

    thanks, Chandra..

  • Chandra,

    I am not sure but you should be able to check pretty easily.

    Regards,

    -Adam