We are facing below problems
1. DRV8825 IC over heat – Taking more current
Under this condition motor Running is OK. But my controller is getting more disturbed and LCD Display totally collapsed. This problem comes when switch on the machine (or can say when power up the mother board)
2. Motor Not Running –
Under this Condition motor only not running. Other functions on my machine are OK working good. I am unable to read pulse output on the winding output (A1 A2 B1 B2). This problem comes after switch ON and setting the machine to run mode.
3. We are facing this problem on multiple numbers of boards. Over 300 nos 96 failures are found.
4. When Replacing IC on driver boards – Few Boards getting OK, Few giving the same above failure no 2.
5. If once the Board getting OK & works good then it is not failure again.