Other Parts Discussed in Thread: DRV8323
Hi,
I am also having fault issues with the DRV8353-EVM. We ran the motor ID process successfully a few times with a maxon motor with hall sensing. At some point, the fault was tripped permanently in the driver chip and we can't run the motor. The driver chip and the 3.3V regulator now heat up immediately upon power-up (bus current = 200mA idle), so it looks like I would have to replace the driver to get the EVM running again.
My main question is if the DRV8353 will be robust enough for our application, seeing as it failed at or below 24V and never drove the small Maxon motor more that 1.5A per phase (usually 500mA or less). Secondarily, I came to the forums to get a better idea of what parts to order now as I troubleshoot, since we are on a schedule.
We are evaluating the driver and FETs so we can run the bus voltage at 60V max comfortably, because the DRV8323 we are using now has thermal runaway issues when operating above 24-30V. We were running this DRV8353-EVM mostly at 12V with the exception of a couple times at 24V.
Thanks,
Jed