This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2510-Q1: The tolerance of GAIN value to DRV2510

Part Number: DRV2510-Q1

Hi teams,

 From the datasheet of DRV2510, the tolerance of gain inside DRV2510 is about +/- 10%. We wonder if it is possible that the gain of IN+ port is +10%, while the IN- side is -10%.

For example, IN+ is 26dB and IN- is 25dB in one driver IC is possible?

Best regards.