Hello,
When testing out the board Q7 and Q5 are now shorted. I was initially having issues in the PWM slow decay mode, the fault LED light up. I believe forward and reverse had the same outcome. Note I was spinning the pot pretty fast. I had a diff probe connected which I noticed the voltage rising probably as much as 30V. The power supply was set to 12V. Now Q7 and Q5 are shorted. I did try spinning the pot fast in the PWM fast decay mode but did not have any issues. Can anyone help explain the draw backs when using slow decay mode?
Thanks,