This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
I have a question to Open Load detection time (tol).
If an open load is removed in a time shorter than tol, will the next open load detection be detected in a time shorter than tol because open load counter is remained?
Or does the open load is detected by same time of tol in the next open load detection?
Regards,
Nishimura
Nishimura-san,
I will need to check with the design team for you. The datasheet does not specify a max deglitch period between clearing and restarting the TOL timer, or if such a mechanism exists (though I suspect there is).
Regards,
Mike
Nishimura-san,
If the current in the winding goes back above 30mA (the open load current threshold) within the Tol window, the timer will clear and restart when current drops below 30mA again.