This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all
Would you mind if we ask DRV8834?
The datasheet shows typical Vtrip accuracy only.
So, how much are the maximum value and the minimum value?
It depends on Xvref, however we assume that it depends on current condition and gain amp toleranace.
In case of using VRERO, we assume that we should consder VFREO's tolerance ±5% and gain amp toleranace.
Kind regards,
Hirotaka Matsumoto
Hi Matsumoto-san,
You can expect the Vtrip accuracy to vary by +/- 2%.
This does not include the VREFO tolerance of of +/- 5%. Total accuracy when using VREFO can be +/- 7%.