We have a J6 8255.J6RevC1_bootlog.txtVayu EVM revision C1 which fails to boot up properly. We see the board hang at various stages of bootup, sometimes at u-boot itself and sometimes during Linux bootup. We are trying a GLSDK 6.04 image which works fine on a revision E1 board that we have.
I have attached a photo of the C1 board , please let me know if the dipswitch settings are okay. We see that there are 2 settings mentioned for SYSBOOT (11100000 10000001 in the Quick Start Guide and 01000100 10000001 in the GLSDK developers guide). We see the same bootup problem with both.
I have also attached the u-boot logs (J6RevC1_bootlog.txt) of one such instance where the board hung during bootup.
What is the difference between these 2 revisions and is there a different u-boot/kernel image required for the C1 ? Will Wi-Fi (using the COM8Q module) work on this board ?
Thanks,
Anurag Maheshwari