Part Number: UCC28180
Other Parts Discussed in Thread: UCC256404, , UCC28056
Hi,
I want to build a Medical SMPS (Class II). Requirements are as follows:
| Input Voltage | 90-264 VAC |
| Input Frequency | 47-63 Hz |
| Output Voltage | 24V |
| Output Current | 4A |
I searched some and found ti Tida series. So i think i need to use PFC (CCM or DCM), HB LCC and synchronous rectifier controller. (And of course mosfets but i did not search them yet)
I'm thinking to use UCC28180D PFC, UC25630-3DDBT or UCC256404 LLC Resonant Controller and UCC24612-2DBVR or UCC24636DBVR synchromous rectifier controller.
For this requirements could i use them or do you recommend another controllers?
Unfortunately price is important.
Best Regards,