This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28180: Medical Switch Mode Power Supply(SMPS)

Part Number: UCC28180
Other Parts Discussed in Thread: UCC256404, , UCC28056

Hi,

I want to build a Medical SMPS (Class II). Requirements are as follows:

Input Voltage 90-264 VAC
Input Frequency 47-63 Hz
Output Voltage 24V 
Output Current 4A

I searched some and found ti Tida series. So i think i need to use PFC (CCM or DCM), HB LCC and synchronous rectifier controller. (And of course mosfets but i did not search them yet)

I'm thinking to use UCC28180D PFC, UC25630-3DDBT or UCC256404 LLC Resonant Controller and UCC24612-2DBVR or UCC24636DBVR synchromous rectifier controller. 

For this requirements could i use them or do you recommend another controllers?

Unfortunately price is important.

Best Regards,