I'm evaluating BQ25672 on EVM.
I'm planning to test this charger chip with external NTC thermistor.
In the datasheet SLUSEB9 in section 8.3.8.5.1, I find formulas on calculating the resistances RT1 and RT2.
But I can't seem to understand how one would get the VT1-VT5 values used in RT1 and RT2 calculations.
Following the datasheet example I can't replicate the resistor RT1 and RT2 values shown in the example.
a) In the datasheet there is NTC_Control_1 register where I can set the VT2, VT3 to a specific % of VREGN.
b) VREGN value is vague. According to the spec it is 5V, but only at VIN=15V. Using 5V value won't give me correct RT values as in datasheet example.
For example datasheet claims, using:
RT2 fixed at 30.31k (to set T5=60deg C)
T1=0deg C setting
RTHcold as 10k 103AT NTC at 0deg is 27.28k
RT1 should then be 5.24k according to the example.
I assume VT1 to be 72% of VREGN during charging (as in datasheet) -> VT1 = 5V*72% = 3.6V ?
This makes RT1 = -10.369k ??
The sentence on page 34 seems to be missing something:
" The [??] provides the comparators with fixed thresholds for VT1 and VT5, and the comparators with programmable
thresholds for VT2 and VT3. "
So how to find values for VT1-VT5 to calculate RT1 and RT2 ?