This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO5852S-Q1: AEC gate drivers

Part Number: ISO5852S-Q1
Other Parts Discussed in Thread: ISO5852S

InsulationCoordination_HVInverter_19052021.pdf

Hello,

We're designing Automotive motor drive with UDC MAX = 880V. Regarding standard we need creepage min. 10mm. All your reinforced isolated gate drivers are specified to work on 5700Vrms, but has creepege only 8mm. How can we use your gate driver in your application if 10mm creepage is needed by standard - check table 4 in attached document. 

Our pullution degree is 2.

Thanks for feedback,

Borut Barbaric

  • Borut, 

    The material group is 1, so the min creepage requirement, per table, is 5mm not 10mm.

    please see Insulation specifications in the datasheet page 7. 

    If this answers your question, please press the green button. 

    Best

    Dimitri

  • Hello,

    This is not true if reinforced insulation is needed. Then creapage is 10mm - read note bellow table 4, taken out of IEC60664-1 standard!

    And ISO5852S is declared as reinforced insulated.

    Regards,

    Borut

  • Hi Borut,

    You are correct. For ISO5852S up to 800V the gate driver is reinforced insulated with 8mm creepage, but at 1kV the driver would be considered as basic insulation. The ISO5852S or the other drivers in our product family would not be able to meet the 10mm creepage requirement.

    Best regards,

    Andy Robles